Ov5640 CSI Camera Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ov5640 CSI Camera Android

1,259 Views
deepanrajanbara
Contributor IV

Hi,

We are currently using custom board based on imx6dl and our OS is android 5.0 lollipop.We are tesing Camera in Android and the configuration is been done and the camera is working.But when the camera is captures still image there is no problem , when we try to record video at 1080p we are getting a pink or a purpule screen we are not sure what is causing this pink screen and recording of 720p video in android there is no problem.Please help as soon us in this Android Camera

0 Kudos
1 Reply

512 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deepanraj 

seems driver does not cover the 1080p option, although it’s theoretically possible to achieve

it would require the coefficient pair values to tweak the frame rate. These coefficient tables

are given by Omnivision. One can check some third party implementations

http://dl.linux-sunxi.org/SDK/A23-v1.0/unpacked/A23/lichee/linux-3.4/drivers/media/video/sunxi-vfe/d... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos