HELP NEEDED TO BUY OLD IMX6 SABRE EVAL KIT (IMX6SDL)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HELP NEEDED TO BUY OLD IMX6 SABRE EVAL KIT (IMX6SDL)

Jump to solution
489 Views
anirudhthabjul
Contributor I

Hello Everyone,

I am Anirudh THABJUL, Electronic engineer working in a company 'Second Bridge', We are situated in Paris.

We have designed our entire schematics from a sub contract company in 2012 using IMX6 SABRE DUAL LITE Eval kit.

Now we want to debugg some major issues which occured while we tried to enable the OPENGL. We are using at present linux version 3.5 which we want to change to some advanced version ex 3.10 which enables OPENGL and QT .

So, In order to do that with existing hardware we need the eval kit with reference IMX6SDL to debug the issues which is designed in 2009 to 2012 and is in obsolete condition now.

Please help me in finding it. It will be very helpful if some one have used eval kit also. We are ready to pay full fare if needed.

Contact

PCBDesign@second-bridge.com

Thank you.

Regards,
Anirudh THABJUL

1 Solution
422 Views
art
NXP Employee
NXP Employee

Since released in 2012, the i.MX6DL SABRE SD board has got no significant hardware changes until now. So, there is no major differences between "old" and "present" i.MX6DL SABRE SD kits.

By the way, please note that enabling OpenGL and so on is generally the matter not of the hardware, but of the software. So, pay attention to the software first. The latest Linux BSP that enables many graphics features including OpenGL and Qt support, is L4.1.15. It is available for download on the NXP web site:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/em...

The related documentation is also available:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/em...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
423 Views
art
NXP Employee
NXP Employee

Since released in 2012, the i.MX6DL SABRE SD board has got no significant hardware changes until now. So, there is no major differences between "old" and "present" i.MX6DL SABRE SD kits.

By the way, please note that enabling OpenGL and so on is generally the matter not of the hardware, but of the software. So, pay attention to the software first. The latest Linux BSP that enables many graphics features including OpenGL and Qt support, is L4.1.15. It is available for download on the NXP web site:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/em...

The related documentation is also available:

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/em...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

422 Views
anirudhthabjul
Contributor I

Thank you so much.

Regards,
Anirudh

0 Kudos