the anolog input voltage range of SD ADC on MPC5775K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the anolog input voltage range of SD ADC on MPC5775K

649 Views
annaxu
Contributor I

Hi,

If there is anyone knows the anolog input voltage range of SD ADC on MPC5775K ? 

Labels (1)
0 Kudos
2 Replies

494 Views
martin_kovar
NXP Employee
NXP Employee

Hi Anna,

SDADC input voltage full scale is 1.2 Vpp (Voltage peak to peak).

pastedImage_1.png

Voltage difference between adcp and adcn can be 1.2V maximally.

Regards,

Martin

0 Kudos

494 Views
annaxu
Contributor I

Hi Martin,

Thank you for your reply ! And do you know the meanings of "number of chirps in a frame" and "the number of samples in a chirp" in the datasheet ??

I think these two sets would affect the sampling of SD ADC , but i'm not sure how they affect.pastedImage_1.png

pastedImage_2.png

0 Kudos