Suggest a board based on i.MX6 Solo for development.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suggest a board based on i.MX6 Solo for development.

439 Views
vipulkumar
Contributor III

Hi,

I need a i.MX6 Solo based board for the development purpose. I will use 

OS - Linux

Yocto - 1.6.1

I have the following requirements:

1. i.MX6 Solo
2. LVDS Display
3. CAN
4. Audio
5. RS485
6. RS232
7. RS422
Can anybody suggest the best board for the above requirements ? 
Also, please share the link and schematic of the board ?
0 Kudos
1 Reply

352 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vipul

one can look at

NXP/Freescale i.MX 6 based Computer on Module - Apalis iMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos