Adv7180 - IMX6 and chromium

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adv7180 - IMX6 and chromium

830 Views
gianlucaromanin
Contributor I

Hi all.

I'm trying to expose the CSI video device with the adv7180 decoder on a IMX6 Solo/Dual (Variscite IMX6 Solo/Dual).

I managed to patch the kernel and the device is running. I can get a gstreamer pipe with:

gst-launch-1.0 imxv4l2videosrc ! imxeglvivsink

and get the parallel camera interface input on the touchscreen (I use a variscite solo CustomBoard EVB with a standard touch). The video is working. I am using an analogic camera attached to the adv7180 and all is now smooth.

I am now trying to get this device working on chromium as a webcam with WebRTC (appr.tc).

The v4l2 device is not used and not seen. If I start chromium with LD_PRELOAD and v4l1compat.so, chromium

seems to access the adv7180 device but it shows a black screen with no apparent error.

I have enabled debug support on my adv7180.c file and with "v4l2-ctl --list-formats-ext" I get nothing from the v4l2 device:

ioctl: VIDIOC_ENUM_FMT

the device is accessed but it seems not to return compatible formats.

Where am I failing?

Any hint?

Labels (4)
0 Kudos
1 Reply

472 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos