AnsweredAssumed Answered

QorIQ GA 16.09 release unable to access meta-nxp-npi or sw-stash.freescale.net, is this needed?

Question asked by pro-supportengineer Employee on Oct 11, 2016
Latest reply on Oct 13, 2016 by pro-supportengineer

After downloading and installing the SDK2.0-1609 release, in sources/meta-nxp-npi-1609/README the following instructions to pull and build SDK2.0-1609 are given.  But the git clone fails because the stash server is unavailable.

 

1) To properly update and build the 1609 release, is it necessary to git clone and link as the instructions indicate below (lines 4 and 5)? 

2) If not required, why are the instructions given?

3) If required, how can customers clone http://sw-stash.freeschale.net if the server is not available per the instructions below?

 

NXP's QorIQ SDK Project
=============================
This is GA 16.09 release which based on SDK v2.0.

 

Steps to build:
1. Install SDK 2.0 source ISO
2. Install SDK 2.0 aarch64 cache ISO #optional, to speed up build
3. $ cd <iso_install_location>/QorIQ-SDK-V2.0-20160527-yocto/sources/
4. $ git clone http://sw-stash.freescale.net/scm/dnyocto/meta-nxp-npi -b jethro-sdk-v2.0-ga-16.09 meta-nxp-npi-ga
5. $ ln -s meta-nxp-npi-ga meta-fsl-local-build #a hack as meta-nxp-npi layer is not included in fsl-setup-env script by default
6. $ cd <iso_install_location>/QorIQ-SDK-V2.0-20160527-yocto/
7. $ . ./fsl-setup-env -m <board>
8. $ bitbake <target>

 

~/neo_mcu_eos-qoriq_v2_sources/sources$ git clone http://sw-stash.freescale.net/scm/dnyocto/meta-nxp-npi -b jethro-sdk-v2.0-ga-16.09 meta-nxp-npi-ga
Cloning into 'meta-nxp-npi-ga'...
fatal: unable to access 'http://sw-stash.freescale.net/scm/dnyocto/meta-nxp-npi/': Could not resolve host: sw-stash.freescale.net

 

How do customer's resolve the host sw-stash.freescale.net?

Outcomes