Is imx6 IPU0 DI1 can't output 1080p@60Hz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is imx6 IPU0 DI1 can't output 1080p@60Hz?

416 Views
weizhunchen
Contributor I

My displayer is  HDMI, and I want to ouput 1080p@60Hz with IPU0_DI1.

Normal circumstances, the pixel clock frequency is 148.5 Mhz, but the actual test value is 113.2 Mhz.

IPU0_DI0, IPU1_DI0, IPU1_DI1 is OK.

Labels (3)
0 Kudos
1 Reply

320 Views
igorpadykov
NXP Employee
NXP Employee

Hi weizhun

this configuration is working fine on sabre ai board, as

IPU0_DI1 is used on sabre ai board (imx6qdl-sabreauto.dtsi)
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos