Hello,
Under Centos 6.4 (64) I installed QorIQ_Linux_SDK_v2.0_SOURCE.iso
and then ran:
cd /opt/nxp/QorIQ-SDK-V2.0-20160527-yocto
./sources/meta-freescale/scripts/host-prepare.sh
. ./fsl-setup-env -m ls1021atwr
bitbake fsl-toolchain
After few minutes I got the attached error log.
Can you help ?
Thank you,
Zvika
Original Attachment has been moved to: log.do_compile.14724.zip
Hello Vered Zvi ,
First please install the Cache binary ISO to void building everything from the scratch.
'__NR_setns' is defined in syscall.h, on your host, installing glibc-devel could help you to overcome this problem.
sudo yum install glibc-devel
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
On page 69 in the SDK user manual, I should run: "cd <S>"
Can you tell how to write it ? There is no folder named <S>.
Thank you,
Zvika
Hello Zvika,
<S> should be source code folder.
For example,
u-boot : build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/u-boot-qoriq/2016.01+fslgit-r0/git/
Linux Kernel: build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/git/
Linux application linux-libc-headers: build_ls1021atwr/tmp/work/cortexa7hf-vfp-neon-fsl-linux-gnueabi/linux-libc-headers/4.1-r0/linux-4.1/
If this is what you need, please copy the whole content here.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
When I did the same under Centos 7 (64) I had no problems.
Thank you,
Zvika