hi, guys:
I can't access the serial port of opensda of s32k144 demo board, the seial driver can't be installed correctly.
here is my device and system information.My system is windows 7 64bit. thanks!
hi, guys:
I can't access the serial port of opensda of s32k144 demo board, the seial driver can't be installed correctly.
here is my device and system information.My system is windows 7 64bit. thanks!
Hi Stanislav,
The customer already did as followed as 'Fixing the USB Drivers | MCU on Eclipse ', but it kept being failed.
Only CDC serial port error occurred, could you check the issue as below?
Best regards,
Kate Lee
Hi,
this looks like a driver issue.
Please check this blog: https://mcuoneclipse.com/2012/10/12/fixing-the-usb-drivers/
Stan