PN532 inCommunicateThru

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 inCommunicateThru

991 Views
juergenschuster
Contributor I

I use the PN532 to read data from a JCOP Card.
With the "inDataExchange" Command, all works fine but this command is very slow (approximately 24 ms per command).
So i changed to the "inCommunicateThru" Command. This command is faster (approximately 10ms per command) but i have some problems.
If i like to read more then 64 Bytes, i receive not all data bytes. I think i must implement chaining, but i dont know how it works. Also in the datasheet there is no information about this command regarding chaining.
Can anybody help me?

I found out that the first databyte (before APDU) from the "inCommunicateThru" Command must be 0x02 or 0x03 (toggle each command). I cannot found any documentation for this byte.
Can anybody help me?

best regard
Juergen

Labels (1)
0 Replies