Hi Everyone,
I'm using T1024RDB board and trying to boot from SD Card. I've prepared SD card based on this document http://www.nxp.com/files/soft_dev_tools/doc/support_info/QORIQ-SDK-2.0-IC-REV0.zip?fasp=1&WT_TYPE=Su... and setted up env with the next values :
=> printenv loadaddr
loadaddr=1000000
=> printenv fdtaddr
fdtaddr=2000000
=> printenv bootfile
bootfile=uImage
=> printenv fdtfile
fdtfile=uImage-t1024rdb.dtb
=> printenv bootcmd
bootcmd=setenv bootargs root=/dev/mmcblk0p2 rw rootdelay=5 console=$consoledev,$baudrate;mmcinfo;ext2load mmc 0:2 0x1000000 /boot/$bootfile;ext2load mmc 0:2 0x2000000 /boot/$fdtfile;bootm 0x1000000 - 0x2000000
After I plugged in a SD, powered on the board and tried to run from the card. I'm getting the next print-out :
.
Hit any key to stop autoboot: 0
Device: FSL_SDHC
Manufacturer ID: 3
OEM: 5344
Name: SD16G
Tran Speed: 25000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.8 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
5469444 bytes read in 526 ms (9.9 MiB/s)
31073 bytes read in 59 ms (513.7 KiB/s)
WARNING: adjusting available memory to 30000000
Wrong Image Format for bootm command
ERROR: can't get kernel image!
From the print-out I can see that two files (uImage and uImage-t1024rdb.dtb) were downloaded successfully and sizes of downloaded files are equal to sizes what actually are on SD card. Looks fine ?! ... I don't know ...
But for some reason I'm getting the error message : Wrong Image Format for bootm command .
Exactly the same uImage and uImage-t1024rdb.dtb files I'm running for TFTP and NFS deployments without any problem.
What am I doing wrong people ?!
Thank you.
Val
The issue is solved.
The problem was in img files on SD card.
Anybody ?!
Val