AnsweredAssumed Answered

DDR3 Script aid question

Question asked by Preetesh Rathod on Oct 3, 2016
Latest reply on Oct 3, 2016 by Yuri Muhin

I would like to point out two things related to DDR3 script aid for IMX6 series.

   1. The current versions of DDR3 scipt aid for all IMX6 series processor does not provide separate Drive strength setting for IMX6 and DDR memory which as per my understanding should be provided. Otherwise we need to change it manually when we are using different strength at IMX6 and at Memory. 

  2. Dynamic ODT is default enabled by this script aid but I think it is better to have option to enable or disable dynamic ODT. Nowhere in the script aid it is mentioned that dynamic ODT is enabled. I think this should be clearly indicated.

 

Let me know what IMX6 team thinks on above two points. 

Outcomes