i.MX7 BOOT_MODE[1:0] power group.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 BOOT_MODE[1:0] power group.

Jump to solution
758 Views
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about i.MX7.
Please see Table 4 in i.MX7 hardware development guide (IMX7DSHDG Rev.0).
As per the Recommendation of No.1 of this table, BOOT_MODE[1:0] power group is VDD_SNVS_IN.
However, I think this is misprint since other documents (Table 88 in IMX7SCEC Rev.2, i.MX7 SABRE schematics) say BOOT_MODE[1:0] power group is NVCC_GPIO1.
Is my understanding correct?


Best Regards,
Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
462 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  "BOOT_MODE0, BOOT_MODE1 and POR_B are connected to NVCC_GPIO1
power domain internally, they shall be pulled up to NVCC_GPIO1, but not VDD_SNVS_IN.
Our EVK schmatic is correct and customers can refer to it for their new projects."

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
463 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  "BOOT_MODE0, BOOT_MODE1 and POR_B are connected to NVCC_GPIO1
power domain internally, they shall be pulled up to NVCC_GPIO1, but not VDD_SNVS_IN.
Our EVK schmatic is correct and customers can refer to it for their new projects."

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 Kudos