checklist for Testing MPC83xx Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

checklist for Testing MPC83xx Board

328 Views
mohsenhaghighat
Contributor III

Hello everybody, We design a few boards with MPC8308. The design is OK, and the boards work good. Now I need to make a checklist method for testing the boards, Because we will produce more numbers of these boards.

Does NXP have any method for this? Can anybody help me? 

0 Kudos
1 Reply

240 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry we do not offer this type document. I think, testing soldering quality and all board components if they properly placed and have desired value - will be enough. The processor itself is 100% tested on factory during production, so I expect it will work if properly soldered. Of course, the exact testing procedure is up to you, for example you can use JTAG boundary scan to test all connections around the processor.

Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos