SoloX Source Series Resistor LVDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SoloX Source Series Resistor LVDS

438 Views
scottgauche
Contributor I

Hi,

Does NXP have any recommendations for adding source series resistance to the LVDS output of the SoloX?  We would like to slow down the edge rates.  We are running the LVDS at 24.58 MHz.

We are trying to lower the amount of 688 MHz (LVDS parent clock) noise we are seeing in emissions scans.  We were able to add 10 pF 0201 capacitors at each LVDS pair between the vias under the SoloX and see the emissions level go down.  But we aren't able to test adding source series resistors because the traces are on internal layers until they reach the connector.

We use a deserializer (DS90CF384) to drive a RGB parallel LCD on another board with 100 ohm termination resistors for each LVDS pair.

This is our LVDS clock tree:

pll5 0 0 688239984 0
pll5_bypass 0 0 688239984 0
pll5_video 0 0 688239984 0
pll5_post_div 0 0 172059996 0
pll5_video_div 0 0 172059996 0
ldb_di0_sel 0 0 172059996 0
ldb_di0_div_7 0 0 24579999 0

Labels (3)
0 Kudos
1 Reply

333 Views
igorpadykov
NXP Employee
NXP Employee

Hi SCOTT

one can look at LVDS common-mode chokes (represent also resistance)

p.13 SPF-27962 i.MX6SX SabreSD schematic

Schematics (1)
IMX6SOLOX-SABRESDB-DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos