Two questions here really about some quirks with using codewarrior.:
1) Everytime I change a setting in the processor expert, the processor expert tree in the left menu disappears. It only comes back after I restart codewarrior.
2) Whenever a new window is opened in the workspace, the windows shifts to the right. Something it shows nothing. Other times, it shows just the recently opened window (such as a new file (.c or .h)). Costs me a lot of time reseting the windows.
Am I doing something wrong? I am using a 4k display, which has given me viewability issues in the past.
Hi Robert Maier
Could you try with the option Reset Perceptive in the window tab?:
After this, select the show view in processor expert options
It should restore the processor expert view. Now to view the component configuration you just click the component. Sometimes when the windows shows nothing you can double-click the window's tab, it will maximize it and update the content, then you can restore it with the same method.
Hope this information help you.
Have a great day,
Jorge Alcala
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you, Jorge. I am using CodeWarrior 5.9. I do not have those options. Any other tips?