imx6 memtool fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 memtool fail

1,506 Views
garyyin
Contributor III

IMX6Solo, linux 3.14.28

I want to check the ASRC(Async Sample Rate Converter) registers, run:

./memtool -32 0x02034000 1
E
Reading 0x1 count starting at add

The cpu hang up。。。

I tested the other module registers such as AUDMUX, it's OK. Why I can't read out the ASRC registers?

Labels (3)
0 Kudos
1 Reply

759 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Hope the following helps.

memtool for i.MX6DP processor 

i.MX6QP Read/Write PCIe register issues by memtool on Yocto 3.14.38_beta 

https://community.nxp.com/message/526001?sr=search&searchId=3145bbe0-f09c-4d90-acb3-8575c8c60465&sea... 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos