KE02Z support on KSDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE02Z support on KSDK

1,208 Views
pablokuziw
Contributor II

We are interested on the KE02Z and configure pins by Pins Tool.

But we cannot find out any KE02Z device information in Pins Tool, then we think that Pins Tool does not support KE02Z.

Are we correct?

If so, do you have a plan to support KE02Z with FRDM-KE02Z40M?

 

Please reply as soon as possible.

 

Best regards,

Pablo

Labels (1)
Tags (2)
2 Replies

1,006 Views
pablokuziw
Contributor II

Hi Erich,

yes, your suggestion it´s well for me. I´m working now with KDS and Processor Expert.

I hope that NXP will include the KE02Z family in KSDK soon.

Best regards,

Pablo

0 Kudos

1,006 Views
BlackNight
NXP Employee
NXP Employee

Hi Pablo,

Yes, this is currently correct. The Pins Tool uses and depends on the Kinetis SDK v2.0. As the Kinetis SDK v2 does not support the KE02Z, the Pins tool cannot support that device. Until there would be the KE02Z supported by the Kinetis SDK v2 (I do not have a date for that), you can use Kinetis Design Studio and Processor Expert to generate the pin muxing and configuration for this device.

I hope this helps,

Erich