IMX6ul elcdif/lcdif linux source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ul elcdif/lcdif linux source

1,065 Views
ameerhamza
Contributor III

Hi all,

I want to ask if the source code is freely available for imx6ul elcdif linux driver. If yes where can i get the source from. Any help would be appreciated.

Thanks,

Am Hamza.

Labels (2)
Tags (2)
0 Kudos
1 Reply

520 Views
igorpadykov
NXP Employee
NXP Employee

Hi Am

please refer to Chapter 12 ELCDIF Frame Buffer Driver

attached Linux Manual, sources link

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/?h=imx_4.1.15_1.0.0_ga

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos