Dear all,
We run AndroidM6.0 demo image on MX6Q-SABRE board.
- Board: MX6Q-SABRE-SD
- Image: android_M6.0.1_2.0.0_image_6dqpsabresd
We try UVC (USB Video Class) camera input.
However, the USB camera is not recognized.
According to the Release Notes(Rev. M6.0.1_2.0.0, 06/2016), BSP supports Media – USB Camera(Logitech(C250 / E3500)).
Does this pre-build image support the USB Camera?
In addition, camera application is not included in this image.
Would you tell me the available camera application for this image?
Best Regards,
Yuuki
Solved! Go to Solution.
Hi yuuki,
In prebuilt image, USB UVC class camera is supported, you should be able to use on console with gstreamer command..
Please there are some issues regarding camera on SDP board, please check the attached document.
Hope this helps.
Dear all,
I’m sorry to be pressing.
Do you have information about this?
Best Regards,
Yuuki