AnsweredAssumed Answered

my system only starts after a second reset

Question asked by Sandro Bastos on Sep 27, 2016
Latest reply on Oct 27, 2016 by Sandro Bastos
Branched to a new discussion

hi,

 

i have a code that boot on twr-vf65gs10, from qspi and running in ddr, i mean, it's stored on qspi non xip mode, then, after reset or power on, vybrid copies the code to ddr and run it - ok, it works fine.

 

the problem: with our own hardware, that is strongly similar to twr, it only runs after a second reset; after power on the system does not start, then i press the reset button and it runs.

 

our hardware manages to boot from qspi since the destination memory is intram, or xip mode; in those cases, the system runs on power on; but if the destination memory is ddr, we need a second reset...

 

the ddr p/n is identical and so is the circuit.

 

has anyone had a similar issue?

 

thank you,

 

Bruno Castelucci

David Seymour

Karina Valencia Aguilar

Mark Middleton

Outcomes