AnsweredAssumed Answered

How to change resolution of LPTMR

Question asked by Alex Wilson Employee on Sep 21, 2016
Latest reply on Sep 25, 2016 by xiangjun.rong

I have a customer with the following question for the KV31, but it may be a more generic Kinetis question:  "

The LPTMR timer is limited to 1ms resolution. It has a minimum value of 4ms (tick_count <= 1 test).  The CPU_LPO_CLK_HZ is currently 1000U.

I need to reconfigure the LPTMR time for 0.5ms resolution with a minimum value 2ms.

What is the best way to do this?"

Outcomes