AnsweredAssumed Answered

Codewarrior fails to work with Ke04z128m4

Question asked by Johan de Vos on Sep 20, 2016
Latest reply on Sep 28, 2016 by Alice_Yang

I had to swap my familiar Codewarrior 10.6 environment to Kinetis Design Studio 3 in order to be able to flash a NXP Kinetis MKE04Z128VLD4 by means of Pemicro Multilink Uni FX.  I tried 'freescale_ke04z128m4_pflash.arp' (version 1.03, 06/02/2014 - also used by KDS) as well as 'ke04z128m4_pflash_pipeline.arp' (version 1.02, 02/07/2014), trying to program the target results in a message "CPROGACMP ERROR 15 DURING SCRIPT".

I installed Coderwarrior 10.7 which specific state to support this chip, but the result is the same.

Can anyone make a suggestion how to make it work in Codewarrior.

Outcomes