Hello,
I'm having trouble on the imx6ul-evk. When I boot off of U-Boot/Linux SD Card included in the kit, I get serial output properly but it locks up randomly. Sometimes it's during the boot process, sometimes it gets all the way to the login screen and I can login.
If I skip the boot and play the the U-Boot environment, it eventually locks up as well. I tried burning the latest image to another card but I get the same issue.
I recompiled U-Boot but using UART2 which I interfaced with via the Arduino headers, but I get the same issue.
Any ideas for future troubleshooting? I could bypass UART and talk to the board over Ethernet, but clearly this remains an annoying issue.
Best,
Louis
Does re-attaching device to the poard help to resync the interface?
Please doublecheck the cable and the connection.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Victor
Reattaching it does resolve it, but only if I reboot the eval board as
well. I have tested this many many times, and yes, the cable is firmly
placed... The replicable problem that I have is that communications are
fine for 1 minute or so and then it goes out.
Best,
Louis