AnsweredAssumed Answered

mpc5646c AN4234

Question asked by jinjingyang Employee on Sep 19, 2016
Latest reply on Sep 20, 2016 by jinjingyang

Dear Sir,

According to AN4234 source code project readme.txt, I can run the script in cygwin to generate M1~M5.

I have installed cygwin and entered tcsh shell.

I can run the script:

"source create_M1_to_M5 2FF8B03C5C5405465A9C94BD2D863279 00000000000000000000000000000000 FFFFFFFFFFFFFFFFFFFFFFFFFFFFFF 4  4 0000001 00"

 

But K1, K2, M2... cannot be generated and is empty. Looks like the four exe in bin directory cannot be executed.

"AES_CMAC_CMD.exe  AES_ENC_CBC_CMD.exe  AES_ENC_ECB_CMD.exe  AES_MP_KDF_CMD.exe"

 

Do you have any comments or suggestions on what I need take into consideration?

 

Regards,

Jason Yang

Outcomes