IS IT POSSIBLE TO USE SDRAM / SRAM WITH KEA SERIES MCU?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IS IT POSSIBLE TO USE SDRAM / SRAM WITH KEA SERIES MCU?

910 Views
brightwang
Contributor III

MY QUESTIONS ARE HERE:

1. IS KINETIS M0+ SUPPORT EXTERNAL MEMORY BUFFER?

2. WHAT IS THE MAX. SIZE UP TO?

3. DOES ANYONE HAS PRACTICE DCASE / SAMPLE CODES?

Labels (1)
3 Replies

679 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bright,

If you want to use SRAM/SDRAM , i'm sorry to say KEA does not have this kind of

interface, it need flex bus moudle which only exist on K series .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

679 Views
brightwang
Contributor III

So Does It Work If I Use I2C / SPI Interface of KEA With RAM Like Cypress's FRAM?http://www.cypress.com/file/41666/download

 

 

Alice_Yang <admin@community.freescale.com> 於 2016/9/19 (週一) 3:46 PM 寫道﹕

#yiv3277776569 * #yiv3277776569 a #yiv3277776569 body {font-family:Helvetica, Arial, sans-serif;}#yiv3277776569 #yiv3277776569 h1, #yiv3277776569 h2, #yiv3277776569 h3, #yiv3277776569 h4, #yiv3277776569 h5, #yiv3277776569 h6, #yiv3277776569 p, #yiv3277776569 hr {}#yiv3277776569 .yiv3277776569button td {}

|

NXP Community

|

Re: IS IT POSSIBLE TO USE SDRAM / SRAM WITH KEA SERIES MCU?

reply from Alice_Yang in CodeWarrior for MCU - View the full discussionHello Bright, If you want to use SRAM/SDRAM , i'm sorry to say KEA does not have this kind ofinterface, it need flex bus moudle which only exist on K series . Hope it helps 

Have a great day,

Alice 

679 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Wang,

From the datasheet of FRAM, i think in theory it can work use the I2C interface,

while there is no demo  .

BR

Alice

0 Kudos