PMIC Selection Guide for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC Selection Guide for i.MX6

Jump to solution
628 Views
marks
Contributor IV

Hello, I need some help selecting the right programming option for the MMPF0100. Looking at the data sheet there are several options (F0, F1, F2 F3,…etc). Is there a table somewhere that shows which "programming option" goes with which i.MX6 part? In particular looking to find the recommended PMIC to go with these:

 

MCIMX6D5EYM10AD, Dual

MCIMX6U5DVM10AC, Dual Lite

 

I think it is the MMPF0100F0AEPR2 but would like a conformation that this is the correct one.

Data sheet:

http://www.nxp.com/files/analog/doc/data_sheet/MMPF0100.pdf?fasp=1&WT_TYPE=Data%20Sheets&WT_VENDOR=F...

 

 

Thanks in advance!

 

Mark

Labels (3)
0 Kudos
1 Solution
457 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mark

recommended selection is given in MMPF0100 Datasheet Table 1.

Orderable Part Variations Column "Reference Designs"

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf

For Dual,DualLite it is F0 option.

Best regards
igor
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
458 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mark

recommended selection is given in MMPF0100 Datasheet Table 1.

Orderable Part Variations Column "Reference Designs"

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf

For Dual,DualLite it is F0 option.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos