imx6dl SCCB slave address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6dl SCCB slave address

726 Views
ifzhao
Contributor I

Dear all,

Recently I've done with ov5645&ov2686 on imx6dl. There is still one annoying problem- the slave address is 0x78 with ov5645, but we finally find it turn out to be 0x3c which is one-bit shift right of 0x78.

Do anyone of you know something about this?

0 Kudos
3 Replies

572 Views
art
NXP Employee
NXP Employee

The I2C address of a peripheral device is defined by a device itself. So, refer to the device (OV5645, OV2686) documentation for the information on its I2C address.


Have a great day,
Artur

0 Kudos

572 Views
ifzhao
Contributor I

The fact is the address on the datasheet do not work out for me. So I probe the bus and find out the correct slave address, and it did work. I wonder why?

Thanks for your reply, though.

0 Kudos

572 Views
art
NXP Employee
NXP Employee

Most likely, you have to specify an I2C address without the read/write bit (LSB of an I2C address). That's why it might look as shifted one bit right.

Best Regards,

Artur

0 Kudos