Hi All,
Now We started to bringup the Marshmallow in Evk6sl board.We are getting the BT issue and not able to update the BT GUI.
Actually for Kitkat we used external/bluetooth/bluedroid folder.But For marshmallow there is no external/bluetooth folder.
Now we are using system/bt folder for Bluetooth Bringup.Is that one is correct or not ?.
Using system/bt folder,we were able to create HCI interface.But every time BT is getting restarted.
LOG ::
01-01 01:45:00.199 430 447 I ActivityManager: Start proc 1001:com.android.bluetooth/1002 for service com.android.bluetooth/.btservice.AdapterService
01-01 01:45:00.202 154 352 W audio_hw_primary: out_set_parameters routing=2, ret 0, out -1242503424
01-01 01:45:00.212 154 351 W audio_hw_primary: ret -32, pcm write 768 error wait error: hw 0x61980 app 0x61f80 avail 0x0
01-01 01:45:00.212 154 351 W audio_hw_primary: : Unknown error -32
01-01 01:45:00.764 1001 1001 D AdapterServiceConfig: Adding HeadsetService
01-01 01:45:00.765 1001 1001 D AdapterServiceConfig: Adding A2dpService
01-01 01:45:00.766 1001 1001 D AdapterServiceConfig: Adding HidService
01-01 01:45:00.766 1001 1001 D AdapterServiceConfig: Adding HealthService
01-01 01:45:00.766 1001 1001 D AdapterServiceConfig: Adding PanService
01-01 01:45:00.766 1001 1001 D AdapterServiceConfig: Adding GattService
01-01 01:45:00.766 1001 1001 D AdapterServiceConfig: Adding BluetoothMapService
01-01 01:45:00.848 430 447 D BluetoothManagerService: Added callback: android.bluetooth.IBluetoothManagerCallback$Stub$Proxy@a4eca42:true
01-01 01:45:00.849 1001 1001 D BluetoothAdapterState: make() - Creating AdapterState
01-01 01:45:00.861 1001 1013 I BluetoothAdapterState: Entering OffState
01-01 01:45:00.871 1001 1001 I bt_bluedroid: init
01-01 01:45:00.880 430 439 I art : Background partial concurrent mark sweep GC freed 9085(578KB) AllocSpace objects, 5(100KB) LOS objects, 33% free, 4MB/7MB, paused 5.434ms total 149.082ms
01-01 01:45:00.909 1001 1014 I bt_bte_conf: bte_load_ble_conf attempt to load ble stack conf from /etc/bluetooth/ble_stack.conf
01-01 01:45:00.911 1001 1014 E bt_osi_config: config_new unable to open file '/etc/bluetooth/ble_stack.conf': No such file or directory
01-01 01:45:00.911 1001 1014 I bt_bte_conf: bte_load_ble_conf file >/etc/bluetooth/ble_stack.conf< not found
01-01 01:45:00.911 1001 1014 I bt_stack_config: init attempt to load stack conf from /etc/bluetooth/bt_stack.conf
01-01 01:45:00.914 1001 1001 I bt_bluedroid: get_profile_interface socket
01-01 01:45:00.925 1001 1017 D BluetoothAdapterProperties: Address is:22:22:B2:97:60:D9
01-01 01:45:00.929 1001 1017 D BluetoothAdapterProperties: Name is: EVK_MX6SL
01-01 01:45:00.945 1001 1001 I bt_bluedroid: get_profile_interface sdp
01-01 01:45:00.954 1001 1012 I bt_bluedroid: config_hci_snoop_log
01-01 01:45:00.955 430 447 D BluetoothManagerService: Broadcasting onBluetoothServiceUp() to 5 receivers.
01-01 01:45:00.966 1001 1013 D BluetoothAdapterState: Current state: OFF, message: 0
01-01 01:45:00.972 1001 1013 D BluetoothAdapterProperties: Setting state to 14
01-01 01:45:00.973 1001 1013 I BluetoothAdapterState: Bluetooth adapter state changed: 10-> 14
01-01 01:45:00.976 1001 1013 D BluetoothBondStateMachine: make
01-01 01:45:00.986 1001 1001 I BtGatt.JNI: classInitNative(L912): classInitNative: Success!
01-01 01:45:00.989 1001 1013 I BluetoothAdapterState: Entering PendingCommandState
01-01 01:45:00.994 1001 1001 D BluetoothAdapterService: getAdapterService() - returning com.android.bluetooth.btservice.AdapterService@48d449f
01-01 01:45:00.998 1001 1018 I BluetoothBondStateMachine: StableState(): Entering Off State
01-01 01:45:00.999 1001 1001 D BtGatt.DebugUtils: handleDebugAction() action=null
01-01 01In onebox_ioctl function
:45:01.000 1001 1001 D BtGatt.Gbt_insert: Initialization function called
attService: Received start requessize of onebox bt_adapter is not 32 byte aligned
t. Starting profile...
01-01 01:bt_insert: Mutex init successfull
45:01.000 1001 1001 D BtGatt.GaInitialising the event cd354894 addr
ttService: start()
01-01 01:45:0In bt_read_reg_params 75 Line
1.006 1001 1001 I bt_bluedroid:02 get_profile_interface gatt
01-060 1 01:45:01.007 1001 1001 D Blue23 toothAdapterService: getAdapterSe32 rvice() - returning com.android.b1a luetooth.btservice.AdapterService0b @48d449f
01-01 01:45:01.007 10054 1 1001 D BtGatt.AdvertiseManager53 : advertise manager created
01-0f6 1 01:45:01.017 1001 1001 V Blue0d toothAdapterState: isTurningOff()4d =false
01-01 01:45:01.017 1001 03 1001 V BluetoothAdapterState: is02 TurningOn()=false
01-01 01:45:0104 .017 1001 1001 V BluetoothAdapt55 erState: isBleTurningOn()=true
000 1-01 01:45:01.026 1001 1001 V B
luetoothAdapterState: isBleTurnin00 gOff()=false
01-01 01:45:01.028 00 1001 1013 D BluetoothAdapterSta
te: Current state: PENDING_COMMAN
HAL CORE_MSG: qos_processor: Queue number = 1
D, message: 4
01-01 01:45:01.028bluez_init: registering with `hci'
1001 1013 I bt_bluedroid: enabWaiting for tx_acces from common hal
le
01-01 01:45:01.029 1001 101bluez_init: done registering `hci0'
4 D bt_stack_manager: event_startonebox_hdev_open: `hci0' open
_up_stack is bringing up the stacusb_host_intf_write_pkt:Successfully written onto card
k.
01-01 01:45:01.045 1001 101In onebox_hdev_send_frame No sufficient head room
4 I bt_hci : start_up
01-01 01:
TXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTX
45:01.058 1001 1014 I bt_vendorTX PACKET LENGTH = 19
: alloc value 0xaf760935
01-01 0HCI_OP_RESET
1:45:01.058 1001 1014 I bt_vend03 or: Redpine vendor init got calle70 d here!!!
a6 2a 0a 00 0c 06 1b 07 a4 1a 00 00 01 00
03 0c 00
TXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTX
Register usb char device interface for BT driverFinished bt char device initialization
HAL CORE_MSG: qos_processor: Queue number = 1
genl-register: nl_family `Obx-BTgenl' asset `bluetooth_asset'
Waiting for tx_acces from common hal
HAS tx_acces from common hal
01-01 01:45:01.283 1001 1014 I usb_host_intf_write_pkt:Successfully written onto card
bt_vendor: Mutyam****protocol ena-process_unaggregated_pkt()
ble
01-01 01:45:01.283 1001 10-process_usb_rcv_pkt()
14 I bt_vendor:
bt_adapter = cd354000
###Received in QNumber:7 Len=6###!!!
06 70 1a 5c bb 4b fa a4 80 00 f8 66 ae 55 04 00
0e 04 01 03 0c 00
RX PACKET LENGTH = 22
COMMAND_COMPLETE_EVENT - HCI_OP_RESET
06 70 1a 5c bb 4b fa a4 80 00 f8 66 ae 55 04 00
HAL CORE_MSG: qos_processor: Queue number = 255
0e 04 01 03 0c 00
RXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRX
HAL CORE_MSG: qos_pro: No More Pkt Due to invalid queueno
@@@ Indicating packet to core:
0e 04
HAL CORE_MSG: qos_processor: Queue number = 255
01 03 0c 00
bt_core_pkt_recv: sending to APP len 6, pkttype 4
HAL CORE_MSG: qos_pro: No More Pkt Due to invalid queueno
onebox_hdev_open: `hci0' open
onebox_hdev_open: device `hci0' already running
rsi_btchr_poll: BT usb char device is pollingQueue front value is: 0
rsi_btchr_poll: BT usb char device is pollingQueue front value is: 0
*************RSI BT READ*********************: 1026
rsi_btchr_read: BT usb char device is readingQueue front value is: 0
Trying to dequeue pkt here: 1026
rsi_btchr_poll: BT usb char device is pollingQueue front value is: -1
Queue front value is: -1
01-01 01:45:02.283 1001 1014 I bt_vendor: ===================>>>>Userial Redpine bluetooth vendor init /dev/rsi
01-01 01:45:02.283 1001 1014 I bt_vendor: ==================>>>> Redpine Vendor OP Code 111111111111111111
01-01 01:45:02.283 1001 1014 I bt_vendor: ==================>>>> Redpine Vendor OP POWER 0
01-01 01:45:02.284 1001 1014 I bt_vendor: ==================>>>> Redpine Vendor OP Code 111111111111111111
01-01 01:45:02.284 1001 1014 I bt_vendor: ==================>>>> Redpine Vendor OP POWER 0
01-01 01:45:02.284 1001 1014 D bt_hci : start_up starting async portion
01-01 01:45:02.284 1001 1021 I bt_hci : event_finish_startup
01-01 01:45:02.284 1001 1021 I bt_hci_h4: hal_open
01-01 01:45:02.284 1001 1021 I bt_vendor: ==================>>>> Redpine Vendor OP Code 111111111111111111
01-01 01:45:02.284 1001 1021 E bt_vendor: ==================>>>> Redpine Vendor OP S_OPEN 3
01-01 01:45:02.293 1001 1021 I bt_vendor: device fd = 48 open
01-01 01:45:02.306 1001 1021 I bt_vendor: ==================>>>> Redpine Vendor OP Code 111111111111111111
01-01 01:45:02.306 1001 1021 E bt_vendor: ==================>>>> Redpine Vendor OP code Default
01-01 01:45:02.324 1001 1021 E bt_hci : hal_says_data_ready ======================================>>>>>>>INCOMING STATE 0
01-01 01:45:02.324 1001 1021 E bt_hci : hal_says_data_ready ======================================>>>>>>>INCOMING STATE 1
01-01 01:45:02.324 1001 1021 E bt_hci : hal_says_data_ready ======================================>>>>>>>INCOMING STATE 2
01-01 01:45:02.325 1001 1021 E bt_hci : hal_says_data_ready ===========================>>>>>>FINISHED STATE IF CASE
01-01 01:45:02.325 1001 1021 W bt_hci : filter_incoming_event ===============CRDGFGYTFRTDCGFCKJH>VR^YFGJHYV KJ^&R==================>>>>>>. opcode: 0xc03.
01-01 01:45:02.325 1001 1021 W bt_hci : filter_incoming_event command complete event with no matching command. opcode: 0xc03.
01-01 01:45:03.299 154 352 W audio_hw_primary: no standby
01-01 01:45:09.049 1001 1016 E bt_hci : startup_timer_expired
01-01 01:45:09.049 1001 1014 E bt_core_module: module_start_up failed to start up "hci_module"
01-01 01:45:09.070 1001 1029 I bt_btu : btu_task pending for preload complete event
01-01 01:45:09.070 1001 1029 I bt_btu_task: Bluetooth chip preload is complete
01-01 01:45:09.070 1001 1029 I bt_btu : btu_task rec*************RSI BT WRITE*********************
eived preload complete event
rsi_btchr_write: BT usb char device is writingSending pkt through HCI device
In onebox_hdev_send_frame No sufficient head room
TXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTX
TX PACKET LENGTH = 19
HCI_OP_RESET
03 70 58 02 6e 20 5d 06 21 00 0e 00 02 00 01 00
03 0c 00
TXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTX
HAL CORE_MSG: qos_processor: Queue number = 1
Waiting for tx_acces from common hal
usb_host_intf_write_pkt:Successfully written onto card
-process_unaggregated_pkt()
-process_usb_rcv_pkt()
bt_adapter = cd354000
###Received in QNumber:7 Len=6###!!!
06 70 00 00 00 00 00 00 00 00 00 00 00 00 04 00
01-01 01:45:09.086 1001 1029 I
HAL CORE_MSG: qos_processor: Queue number = 255
: BTE_InitTraceLevels --
HAL CORE_MSG: qos_pro: No More Pkt Due to invalid queueno
TRC_HCI
0e 04 01 03 0c 00
RX PACKET LENGTH = 22
COMMAND_COMPLETE_EVENT - HCI_OP_RESET
06 70 00 00 00 00 00 00 00 00 00 00 00 00 04 00
0e 04 01 03 0c 01-01 01:45:09.086 1001 1029 I 00 : BTE_InitTraceLevels --
TRC_L2CAP
01-01 01:45:09.086 10
RXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRX
01 1029 I : BTE_InitTraceLevels -- TRC_RFCOMM
01-01 01:@@@ Indicating packet to core:
04 09.086 1001 1029 I :0e BTE_InitTraceLevels -- TRC_AVDT
01-01 01:45:09.086 1001 1029 I01 : BTE_InitTraceLevels --03 TRC_AVRC
01-01 01:45:09.086 100c 01 1029 I : BTE_InitTrac00 eLevels -- TRC_A2D
01-01 01:45:0
9.086 1001 1029 I : BTEbt_core_pkt_recv: sending to APP len 6, pkttype 4
_InitTraceLevels -- TRC_BNEP
01-01 01:45:09.086 1001 1029 I : BTE_InitTraceLevels -- TRC_BTM
01-01 01:45:09.086 1001 1029 I : BTE_InitTraceLevels -- TRC_GAP
01-01 01:45:09.086 1001 1029 I : BTE_InitTraceLevels -- TRC_PAN
01-01 01:45:09.086 1001 1029 I : BTE_InitTraceLevels -- TRC_SDP
01-01 01:45:09.086 1001 1029 I : BTE_InitTraceLevels -- TRC_GATT
01-01 01:45:09.086 1001 1029 I : BTE_InitTraceLevels -- TRC_SMP
01-01 01:45:09.086 1001 1029 I : BTE_InitTraceLevels -- TRC_BTAPP
01-01 01:45:09.086 1001 1029 I : BTE_InitTraceLevels -- TRC_BTIF
01-01 01:45:09.089 1001 1021 E bt_hci : ==================================>>>>>> Adding the Wait entry opcode 0xc03
onebox_hdev_flush: `hci0' flush
onebox_hdev_close: `hci0' close
01-01 01:45:13.031 1001 1013 D BluetoothAdapterState: Current state: PENDING_COMMAND, message: 101
01-01 01:45:13.032 1001 1013 E BluetoothAdapterState: Error enabling Bluetooth (enable timeout)
01-01 01:45:13.032 1001 1013 D BluetoothAdapterProperties: Setting state to 10
01-01 01:45:13.032 1001 1013 I BluetoothAdapterState: Bluetooth adapter state changed: 14-> 10
01-01 01:45:13.034 430 447 E BluetoothManagerService: recoverBluetoothServiceFromError
01-01 01:45:13.049 1001 1013 I BluetoothAdapterState: Entering OffState
01-01 01:45:13.060 883 883 W ContextImpl: Calling a method in the system process without a qualified user: android.app.ContextImpl.startService:1221 android.content.ContextWrapper.startService:581 and
01-01 01:45:13.098 883 997 D Index : Deleting data for locale 'en_US' took 2 millis
01-01 01:45:13.113 883 883 D DockEventReceiver: finishStartingService: stopping service
01-01 01:45:13.161 883 997 D Index : Indexing locale 'en_US' took 63 millis
01-01 01:45:13.552 1001 1013 D BluetoothAdapterState: Current state: OFF, message: 23
01-01 01:45:13.554 430 447 D BluetoothManagerService: Broadcasting onBluetoothServiceDown() to 5 receivers.
01-01 01:45:13.567 1001 1001 W BluetoothSdpJni: Cleaning up Bluetooth SDP Interface...
01-01 01:45:13.567 1001 1001 W BluetoothSdpJni: Cleaning up Bluetooth Health object
01-01 01:45:13.567 1001 1001 I BluetoothServiceJni: cleanupNative: return from cleanup
01-01rsi_btchr_close: BT usb char device is closing 01:45:13.572 1001 1001 I art onebox_hdev_flush: `hci0' flush
: System.exit called, status: onebox_hdev_close: `hci0' close
0
01-01 01:45:13.572 1001 1001onebox_hdev_close: device `hci0' not running
I AndroidRuntime: VM exiting with result code 0, cleanup skipped.
01-01 01:45:13.633 430 859 I ActivityManager: Process com.android.bluetooth (pid 1001) has died
01-01 01:45:13.633 430 859 W ActivityManager: Scheduling restart of crashed service com.android.bluetooth/.gatt.GattService in 1000ms
01-01 01:45:16.566 430 447 D BluetoothManagerService: MESSAGE_RESTART_BLUETOOTH_SERVICE: Restart IBluetooth service
01-01 01:45:16.592 430 447 I ActivityManager: Start proc 1033:com.android.bluetooth/1002 for service com.android.bluetooth/.btservice.AdapterService
01-01 01:45:16.735 1033 1033 D AdapterServiceConfig: Adding HeadsetService
01-01 01:45:16.735 1033 1033 D AdapterServiceConfig: Adding A2dpService
01-01 01:45:16.735 1033 1033 D AdapterServiceConfig: Adding HidService
01-01 01:45:16.735 1033 1033 D AdapterServiceConfig: Adding HealthService
01-01 01:45:16.736 1033 1033 D AdapterServiceConfig: Adding PanService
01-01 01:45:16.736 1033 1033 D AdapterServiceConfig: Adding GattService
01-01 01:45:16.736 1033 1033 D AdapterServiceConfig: Adding BluetoothMapService
01-01 01:45:16.753 430 447 D BluetoothManagerService: Added callback: android.bluetooth.IBluetoothManagerCallback$Stub$Proxy@4f1aea7:true
01-01 01:45:16.754 1033 1033 D BluetoothAdapterState: make() - Creating AdapterState
01-01 01:45:16.758 1033 1033 I bt_bluedroid: init
01-01 01:45:16.759 1033 1045 I BluetoothAdapterState: Entering OffState
01-01 01:45:16.762 1033 1046 I bt_bte_conf: bte_load_ble_conf aIn onebox_ioctl function
ttempt to load ble stack conf from /etc/bluetooth/ble_stack.conf
01-01 01:45:16.762 1033 1046 E bt_osi_config: config_new unable to open file '/etc/bluetooth/ble_stack.conf': No such file or directory
01-01 01:45:16.762 1033 1046 I bt_bte_conf: bte_load_ble_conf file >/etc/bluetooth/ble_stack.conf< not found
01-01 01:45:16.762 1033 1046 I bt_stack_config: init attempt to load stack conf from /etc/bluetooth/bt_stack.conf
01-01 01:45:16.763 1033 1033 I bt_bluedroid: get_profile_interface socket
01-01 01:45:16.765 1033 1033 I bt_bluedroid: get_profile_interface sdp
01-01 01:45:16.771 1033 1043 I bt_bluedroid: config_hci_snoop_log
01-01 01:45:16.772 430 447 D BluetoothManagerService: Broadcasting onBluetoothServiceUp() to 5 receivers.
01-01 01:45:16.776 1033 1045 D BluetoothAdapterState: Current state: OFF, message: 0
01-01 01:45:16.776 1033 1045 D BluetoothAdapterProperties: Setting state to 14
01-01 01:45:16.776 1033 1045 I BluetoothAdapterState: Bluetooth adapter state changed: 10-> 14
01-01 01:45:16.778 1033 1045 D BluetoothBondStateMachine: make
01-01 01:45:16.781 1033 1049 D BluetoothAdapterProperties: Address is:22:22:B2:97:60:D9
01-01 01:45:16.786 1033 1049 D BluetoothAdapterProperties: Name is: EVK_MX6SL
01-01 01:45:16.792 1033 1033 I BtGatt.JNI: classInitNative(L912): classInitNative: Success!
01-01 01:45:16.795 1033 1033 D BluetoothAdapterService: getAdapterService() - returning com.android.bluetooth.btservice.AdapterService@48d449f
01-01 01:45:16.795 1033 1050 I BluetoothBondStateMachine: StableState(): Entering Off State
01-01 01:45:16.796 1033 1045 I BluetoothAdapterState: Entering PendingCommandState
01-01 01:45:16.797 1033 1033 D BtGatt.DebugUtils: handleDebugAction() action=null
01-01 01:45:16.798 1033 1033 D BtGatt.GattService: Received start request. Starting profile...
01-01 01:45:16.798 1033 1033 D BtGatt.GattService: start()
01-01 01:45:16.798 1033 1033 I bt_bluedroid: get_profile_interface gatt
01-01 01:45:16.800 1033 1033 D BluetoothAdapterService: getAdapterService() - returning com.android.bluetooth.btservice.AdapterService@48d449f
01-01 01:45:16.800 1033 1033 D BtGatt.AdvertiseManager: advertise manager created
01-01 01:45:16.807 1033 1033 V BluetoothAdapterState: isTurningOff()=false
01-01 01:45:16.808 1033 1033 V BluetoothAdapterState: isTurningOn()=false
01-01 01:45:16.808 1033 1033 V BluetoothAdapterState: isBleTurningOn()=true
01-01 01:45:16.808 1033 1033 V BluetoothAdapterState: isBleTurningOff()=false
01-01 01:45:16.809 1033 1045 D BluetoothAdapterState: Current state: PENDING_COMMAND, message: 4
01-01 01:45:16.809 1033 1045 I bt_bluedroid: enable
01-01 01:45:16.809 1033 1046 D bt_stack_manager: event_start_up_stack is bringing up the stack.
01-01 01:45:16.809 1033 1046 I bt_hci : start_up
01-01 01:45:16.816 1033 1046 I bt_vendor: alloc value 0xaf760935
01-01 01:45:16.817 1033 1046 I bt_vendor: Redpine vendor init got called here!!!
01-01 01:45:16.838 1033 1046 I bt_vendor: Mutyam****protocol enable
01-01 01:45:16.838 1033 1046 I bt_vendor:
01-01 01:45:17.549 430 443 I ActivityManager: Start proc 1055:com.android.musicfx/u0a10 for broadcast com.android.musicfx/.ControlPanelReceiver
01-01 01:45:17.552 430 859 I MediaFocusControl: AudioFocus abandonAudioFocus() from android.media.AudioManager@f247743com.android.music.MediaPlaybackService$3@faf61c0
01-01 01:45:17.655 1055 1055 W System : ClassLoader referenced unknown path: /system/priv-app/MusicFX/lib/arm
01-01 01:45:17.658 1055 1055 V MusicFXControlPanelReceiver: onReceive
01-01 01:45:17.658 1055 1055 V MusicFXControlPanelReceiver: Action: android.media.action.CLOSE_AUDIO_EFFECT_CONTROL_SESSION
01-01 01:45:17.658 1055 1055 V MusicFXControlPanelReceiver: Package name: com.android.music
01-01 01:45:17.659 1055 1055 V MusicFXControlPanelReceiver: Audio session: 8
01-01 01:45:17.660 1055 1055 V MusicFXControlPanelEffect: closeSession(android.app.ReceiverRestrictedContext@9ab85a8, com.android.music, 8)
onebox_hdev_open: `hci0' open
rsi_btchr_poll: BT usb char device is pollingQueue front value is: 0
rsi_btchr_poll: BT usb char device is pollingQueue front value is: 0
*************RSI BT READ*********************: 1026
rsi_btchr_read: BT usb char device is readingQueue front value is: 0
Trying to dequeue pkt here: 1026
rsi_btchr_poll: BT usb char device is pollingQueue front value is: -1
Queue front value is: -1
01-01 01:45:17.838 1033 1046 I bt_vendor: ===================>>>>Userial Redpine bluetooth vendor init /dev/rsi
01-01 01:45:17.838 1033 1046 I bt_vendor: ==================>>>> Redpine Vendor OP Code 111111111111111111
01-01 01:45:17.838 1033 1046 I bt_vendor: ==================>>>> Redpine Vendor OP POWER 0
01-01 01:45:17.838 1033 1046 I bt_vendor: ==================>>>> Redpine Vendor OP Code 111111111111111111
01-01 01:45:17.839 1033 1046 I bt_vendor: ==================>>>> Redpine Vendor OP POWER 0
01-01 01:45:17.839 1033 1046 D bt_hci : start_up starting async portion
01-01 01:45:17.839 1033 1053 I bt_hci : event_finish_startup
01-01 01:45:17.839 1033 1053 I bt_hci_h4: hal_open
01-01 01:45:17.839 1033 1053 I bt_vendor: ==================>>>> Redpine Vendor OP Code 111111111111111111
01-01 01:45:17.839 1033 1053 E bt_vendor: ==================>>>> Redpine Vendor OP S_OPEN 3
01-01 01:45:17.842 1033 1053 I bt_vendor: device fd = 48 open
01-01 01:45:17.862 1033 1053 I bt_vendor: ==================>>>> Redpine Vendor OP Code 111111111111111111
01-01 01:45:17.862 1033 1053 E bt_vendor: ==================>>>> Redpine Vendor OP code Default
01-01 01:45:17.872 1033 1053 E bt_hci : hal_says_data_ready ======================================>>>>>>>INCOMING STATE 0
01-01 01:45:17.872 1033 1053 E bt_hci : hal_says_data_ready ======================================>>>>>>>INCOMING STATE 1
01-01 01:45:17.872 1033 1053 E bt_hci : hal_says_data_ready ======================================>>>>>>>INCOMING STATE 2
01-01 01:45:17.872 1033 1053 E bt_hci : hal_says_data_ready ===========================>>>>>>FINISHED STATE IF CASE
01-01 01:45:17.872 1033 1053 W bt_hci : filter_incoming_event ===============CRDGFGYTFRTDCGFCKJH>VR^YFGJHYV KJ^&R==================>>>>>>. opcode: 0xc03.
01-01 01:45:17.872 1033 1053 W bt_hci : filter_incoming_event command complete event with no matching command. opcode: 0xc03.
^C
130|root@evk_6sl:/ # *************RSI BT WRITE*********************
rsi_btchr_write: BT usb char device is writingSending pkt through HCI device
In onebox_hdev_send_frame No sufficient head room
TXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTX
TX PACKET LENGTH = 19
HCI_OP_RESET
03 70 00 00 f6 03 1d 00 3b 00 00 00 71 10 01 00
03 0c 00
TXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTX
HAL CORE_MSG: qos_processor: Queue number = 1
Waiting for tx_acces from common hal
usb_host_intf_write_pkt:Successfully written onto card
-process_unaggregated_pkt()
-process_usb_rcv_pkt()
bt_adapter = cd354000
###Received in QNumber:7 Len=6###!!!
06 70 00 00
HAL CORE_MSG: qos_processor: Queue number = 255
HAL CORE_MSG: qos_pro: No More Pkt Due to invalid queueno
00 00 00 00 00 00 00 00 00 00 04 00
0e 04 01 03 0c 00
RX PACKET LENGTH = 22
COMMAND_COMPLETE_EVENT - HCI_OP_RESET
06 70 00 00 00 00 00 00 00 00 00 00 00 00 04 00
0e 04 01 03 0c 00
RXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRX
@@@ Indicating packet to core:
0e 04 01 03 0c 00
bt_core_pkt_recv: sending to APP len 6, pkttype 4
rsi_btchr_close: BT usb char device is closingonebox_hdev_flush: `hci0' flush
onebox_hdev_close: `hci0' close
In onebox_ioctl function
onebox_hdev_open: `hci0' open
rsi_btchr_poll: BT usb char device is pollingQueue front value is: 0
rsi_btchr_poll: BT usb char device is pollingQueue front value is: 0
*************RSI BT READ*********************: 1026
rsi_btchr_read: BT usb char device is readingQueue front value is: 0
Trying to dequeue pkt here: 1026
rsi_btchr_poll: BT usb char device is pollingQueue front value is: -1
Queue front value is: -1
*************RSI BT WRITE*********************
rsi_btchr_write: BT usb char device is writingSending pkt through HCI device
In onebox_hdev_send_frame No sufficient head room
TXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTX
TX PACKET LENGTH = 19
HCI_OP_RESET
03 70 15 00 72 20 78 42 05 00 0c 16 1f 16 01 00
03 0c 00
TXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTXTX
HAL CORE_MSG: qos_processor: Queue number = 1
Waiting for tx_acces from common hal
usb_host_intf_write_pkt:Successfully written onto card
-process_unaggregated_pkt()
-process_usb_rcv_pkt()
bt_adapter = cd354000
###Received in QNumber:7 Len=6###!!!
06 70 00 00
HAL CORE_MSG: qos_processor: Queue number = 255
HAL CORE_MSG: qos_pro: No More Pkt Due to invalid queueno
00 00 00 00 00 00 00 00 00 00 04 00
0e 04 01 03 0c 00
RX PACKET LENGTH = 22
COMMAND_COMPLETE_EVENT - HCI_OP_RESET
06 70 00 00 00 00 00 00 00 00 00 00 00 00 04 00
0e 04 01 03 0c 00
RXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRXRX
@@@ Indicating packet to core:
0e 04 01 03 0c 00
bt_core_pkt_recv: sending to APP len 6, pkttype 4
rsi_btchr_close: BT usb char device is closingonebox_hdev_flush: `hci0' flush
onebox_hdev_close: `hci0' close
In onebox_ioctl function
onebox_hdev_open: `hci0' open
rsi_btchr_poll: BT usb char device is pollingQueue front value is: 0
rsi_btchr_poll: BT usb char device is pollingQueue front value is: 0
*************RSI BT READ*********************: 1026
rsi_btchr_read: BT usb char device is readingQueue front value is: 0
Trying to dequeue pkt here: 1026
rsi_btchr_poll: BT usb char device is pollingQueue front value is: -1
Queue front value is: -1
How to solve this issue and how to update the android GUI.
Any Solution ?
Thanks in Advance.