New to kinetis and need to do a quick project with K21_LK5. For the development environment, I will need a multilink interface and (maybe a free version since it will be below 64k) CodeWarrior® for MCUs (Eclipse IDE), right? Or, an IDE from IAR? Any comments are greatly appreciated!!!
Hi Gary,
you use K21 I suggest you use KDS3.2 which is a free SW without code size limitation
Kinetis Design Studio Integrated Development Environment (IDE)|NXP
or you can also use CW10.7
CodeWarrior for Microcontrollers-Eclipse IDE|NXP
the CW special edition (free version) has 64KB code and data size limit for Kinetis E,L,M Series
for more information, see http://cache.nxp.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------