i.MX6UL从eMMC启动出现问题。

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL从eMMC启动出现问题。

Jump to solution
1,868 Views
luluxu
Contributor II

imx6ul evk 的底板(原理图编号是:SCH-28616)+ SCH-29090的核心板;

Linux版本是3.14.52 ;

使用MFGtools烧写时,没有报错,串口也能正常输出。

烧录成功后从eMMC启动时,串口无任何打印信息,过一段时间后,i.MX6ul 自动变到烧录模式。

这可能是什么原因导致的?

谢谢!

Labels (2)
0 Kudos
1 Solution
785 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
3 Replies
785 Views
igorpadykov
NXP Employee
NXP Employee

Q: i.MX6UL problem with booting from eMMC.
imx6ul evk floor (diagram number is: SCH-28616) + SCH-29090 core board;
Linux version is 3.14.52;
When using MFGtools programming, there is no error, the serial port can be normal output.
After the successful launch of programming from eMMC, serial no printed information, after some time, i.MX6ul automatically change to the programming mode.
What could be the causes?

A: Had you run ddr test for custom board?

https://community.freescale.com/docs/DOC-105652 

https://community.nxp.com/docs/DOC-331528

after test please rebuild uboot with new calibration settings in *.cfg

file, set correct ddr size in uboot/include/configs/*board*.h file.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
785 Views
luluxu
Contributor II

Hi Igor,

   Thanks for your help.

   I  did the ddr test, It's no use.

   And,The board is made by NXP,  the PCB version is SCH-29090_REV_C.

0 Kudos
786 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos