AnsweredAssumed Answered

License restriction

Question asked by Denny Kluts on Sep 13, 2016

Hi,

 

I have installed LPCexpresso (Version: LPCXpresso v5.0.14 [Build 1109] [2012-12-19] ) on a WindowsXP SP3 machine,
and build a project", then try to start debug.

 

But the dialog says,

 

"License restriction: Flash image too large for this license."

 

and can't run it. I found similar answers on the forum.

 

The popup "Hello World" works, I have tested this.

I have also checked the license keys.

  • HKEY_CURRENT_USER\Software\Microsoft\Windows Script Host\Settings\Enabled
  • HKEY_LOCAL_MACHINE\Software\Microsoft\Windows Script Host\Settings\Enabled

They are correct!

 

I have made a zip file of the license folder and attached it, because other persons had to do the same. Also the .log file is included. Please help so I am able to run my project.

 

Best regards

Original Attachment has been moved to: LPCXpresso.zip

Original Attachment has been moved to: .log.zip

Outcomes