Hello,
I have a FRDM-KL43Z development board. I would like to know if it's possible to use the OpenSDA to communicate like a serial port with the target processor ?
I see correctly the created port COM (CDC Serial Port) in Device manager and I can enter inside like a storage G: (I see the HTML, TXT, CAT and INF files).
I'm able to open the port COM with the software "Hercules", so I imagine I can send data but I don't see how to retrieve the data in my MCU. I tried to add a UART with Processor Expert but UART0 is not available (only the UART2).
Best regards,
Sam,
Solved! Go to Solution.
Hi,
Thank you, it's OK. I was misled by the schemtic of the kit where it's noted UART0 and not LPUART0, so I didn't see the UART0 when I added a fsl_uart, with fsl_lpuart it's OK.
Sorry for the trouble,
Sam,
Hi,
Thank you, it's OK. I was misled by the schemtic of the kit where it's noted UART0 and not LPUART0, so I didn't see the UART0 when I added a fsl_uart, with fsl_lpuart it's OK.
Sorry for the trouble,
Sam,
Hi, Sam,
Of course, you can use the USB CDC as a serial COM to communicate with KL43 on FRDM-KL43Z, pls refer to schematics of FRDM-KL43, the PTA1(PTA1/UART0_RX/TPM2_CH0) and PTA2(PTA2/UART0_TX/TPM2_CH1) pins are used as the SCI port(using uart0). Pls programe the uart0 so that it can communicate as serial port.
I suggest you download SDK2.0 based on KL43 from the website:
You can use the Hello_World as the example.
C:\Freescale\SDK2.0KL43Z256\boards\frdmkl43z\demo_apps\hello_world in SDK2.0 tools
Hope it can help you
BR
Xiangjun Rong