I am working with LPC54102 to transfer data from certain buffers to the GPIO outputs.
The time is critical and I do not need interrupts each time a DMA transfer needs to be triggered.
Is it enough to program a timer (that can trigger a DMA channel) with a match value, and each time the TC will match that value a flag will trigger the DMA without interrupting (and going into the ISR in order to clear the interrupt)?
I would really appreciate your answer.
Thank you,
Doini
Hi Doini
Did you ever get this figured out? I am doing the same thing. I believe that there should be no interrupt necessary and that the match should be able to trigger the DMA unrelated to the exernal match pins. I have not been able to get this to work but I think that I am close. I posted a question about this including my LPCOpen code yesterday called "Cannot get DMA triggered with Timer Match".
Good Luck - James