AnsweredAssumed Answered

i.MX6 board - Technical questions

Question asked by Kevin CHAPPUIS on Sep 11, 2016
Latest reply on Sep 12, 2016 by Kevin CHAPPUIS

Hello,

 

I'm looking for a hardware platform based on ARM architecture for automotive applications. After reading documents around the i.MX6 family, I have several technical questions to clarify some points in order to confirm if the i.MX6 can be a potential solution:

 

    1. Is it possible to restrict peripheral accesses only from the ARM Secure world with a hardware IP such as ARM CoreLink NIC-400?

    2. Which is the GIC (Generic Interrupt Controller) version and revision?

    3. Is it possible to have access to all ARM processors modes (secure PL1, monitor) in order to implement custom applications? If so, how this custom binary can be added in the BSP during the flash process?

 

Thanks for your support.

 

Best Regards,

Kevin

Outcomes