Hi,
I am bit confuse about SIM interface on iMX6UL.
As per technical reference manual page # 2799, "The SIM module has one port that can be used to interface with the various cards." But block diagram shows two port, 0 & 1.
Referred i.MX6UL pin muxing, Found that there are four ports.
SIM1.Port0,
SIM1.Port1,
SIM2.Port0,
SIM2.Port1.
Will appreciate any help or clarification for understanding above with reference if any.
Can you please let me know on which two SIM ports i can connect smart card? As datasheet shows upto 2 SIM interface support.
Thanks,
Ritesh
Hello,
Please refer to https://community.nxp.com/thread/434369
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------