AnsweredAssumed Answered

Integration issue when adding McuOnEclipse FreeRTOS component

Question asked by ahmed hrabi on Sep 9, 2016
Latest reply on Sep 13, 2016 by Erich Styger

Hello everyone, 

 

I'am triying to create a processor expert project with sdk1.3, MK60DN512VLL10 Micro-proc in a custom board. I need to add the mcuoneclipse freeRTOS component to my project and i was following this tutorial : 

 

https://mcuoneclipse.com/2015/07/08/tutorial-using-processor-expert-and-freertos-with-kinetis-sdk-v1-2/ 

 

I added the component in the components library, but when i add the freeRTOS to the project this error occured  :

 

The compiler have no suggestions even when i changed the Cross ARM C compiler Preprocessor to: “FSL_RTOS_FREE_RTOS”. 

Have anyone any idea about this ? 

 

Thanks. 

 

Outcomes