AnsweredAssumed Answered

Can't choose SCI1 device on MagniV Device (S12ZVCA)

Question asked by Jesse Robinson on Sep 9, 2016
Latest reply on Jul 1, 2018 by Aaron Lee

I'm trying to set up a project for the S12ZVCA processor and can't seem to set up the SCI1 peripheral in processor expert, it's not a selectable option in processor expert.  If I don't choose anything under device, then I can select the RX1 and TX1 pins, but then I get the error about not having a device selected and can't generate the code or make an interrupt, when I try and choose a device, there is not SCI1 option and then the RX1 and TX1 pins are gone. I'm using Codewarrior 10.7.0

 

Thanks,

Outcomes