adb reboot is not working on imx6 sabre lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adb reboot is not working on imx6 sabre lite

649 Views
sumanthg
Contributor II

adb reboot is not working

when i type adb reboot in the terminal. the devices is going to off but it is unable to start. I need to restart manually.

How can i resolve this issue.

Labels (2)
0 Kudos
3 Replies

510 Views
igorpadykov
NXP Employee
NXP Employee

Hi sumanth

for reliable reboot pmic also should be restarted as it is done

in nxp Sabre SD schematic spf-27392 p.19,21 with signals PWRON

U507. So one can check if similar solution is used on board.

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

510 Views
sumanthg
Contributor II

In Sabre lite, there is no PMIC,So without PMIC there is any possibility to do reliable reboot.

0 Kudos

510 Views
sumanthg
Contributor II

In Sabre lite, there is no PMIC,So without PMIC there is any possibility to do reliable reboot.

0 Kudos