New Features of L3.10.53_1.1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New Features of L3.10.53_1.1.0

482 Views
eishishibusawa
Contributor III

Dear Sir

I want to ask you about the description of new features.

I refer to the i.MX Linux Release Notes, Rev L3.10.53_1.1.0-ga, 01/2015.

It is described the new features of L3.10.53_1.1.0.

 

Q1.

Can I understand that the new features are compared with L3.10.17_1.0.3?

 

Best Regards,

Eishi SHIBUSAWA

Labels (4)
0 Kudos
3 Replies

369 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Eishi,

the quick answer is yes. In general the 'New Features' described in the Release notes are compared to the previous release. Just please note that the documentation format changed form 3.10.17 to 3.10.53. In the first one there was a release Note for the different boards and in the second there is a general release notes document.

If you have any question please let me know.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

369 Views
eishishibusawa
Contributor III

Dear Carlos

 

Thank you for quick reply.

Can I ask you one more question?

 

I think that the final version of L3.10.17 is L L3.10.17_1.0.3.

I understand that the L3.10.17_1.0.3 is the patch for L3.10.17_1.0.0.

 

Q1.

Can I understand that L3.10.53_1.1.0 contains the improved issues with L3.10.17_1.0.3?

 

Best Regards,

Eishi SHIBUSAWA

 

0 Kudos

369 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Eishi,

sure, you can compare each release with the last patch of last version.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------