MMDC IO mux information for LPDDR3 for i.MX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMDC IO mux information for LPDDR3 for i.MX7D

Jump to solution
1,269 Views
yuuki
Senior Contributor II

Dear all,

We want to connect LPDDR3 to i.MX7D.


We referred to Muxing Options of the reference manual.
http://www.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf
  - 8.1.1.1 Muxing Options

However, we think that this is the IO name for DDR3.


May we have MMDC IO mux information for LPDDR3?
or
Is there the schematic of LPDDR3 connection which NXP recommends?


Would you confirm whether the table which we made is correct when there is not these information?


Best Reagrds,
Yuuki

Labels (1)
0 Kudos
1 Solution
966 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Basically it is possible to use the WaRP7 design.

Also I have sent You NXP schematic for validation board via e-mail.

Hope it helps.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

5 Replies
966 Views
yuuki
Senior Contributor II

Dear NXP support,

We found a Schematics for WaRP7.
In WaRP7, i.MX7Solo and LPDDR3 are used.

https://www.element14.com/community/docs/DOC-82961/l/design-file-for-warp7-board-schematics-pcb-layo...

About connection of LPDDR3, is this the Schematic which NXP recommends?

May I have advice?

Best Regards,
Yuuki

967 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Basically it is possible to use the WaRP7 design.

Also I have sent You NXP schematic for validation board via e-mail.

Hope it helps.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

966 Views
federiconatali
Contributor I

Hi, I'm new of the community. I also need to connect a LPDDR2 (1Gb x32) to i.MX7D, thus I wish to ask if the warp7 schematic is the recommend one, and/or if you can send a NXP schematic for validation board. 

Thanks.

0 Kudos
966 Views
Yuri
NXP Employee
NXP Employee

Hello, Natali!

As for  "if the warp7 schematic is the recommend one" - yes , customers can use it. 

Regards,

Yuri.

0 Kudos
966 Views
yuuki
Senior Contributor II

Dear Natali-san,

I'm sorry for the delay in my response.

Unfortunately, I cannot send NXP schematic for validation board to you, because  I think that it is under NDA.

If you need it, I recommend that you contact to Yuri-san.

Best Regards,
Yuuki

0 Kudos