AnsweredAssumed Answered

USB hub driver on i.Mx6 QP kernel

Question asked by Jaffin MK on Sep 5, 2016
Latest reply on Sep 14, 2016 by Jaffin MK

Hello

 

We are trying to build a custom board for a smart device using iMX6QP application processor. Since we needed to expand the USB functionality of the processor we have decided to use a USB hub chip (SMSC USB2514). Now I have found that there are other custom boards which has used this same chip with the imx6 processor, but I need to confirm that the driver for the same is available in the kernel that I have downloaded from the git link of the freescale imx6 kernel. (linux-2.6-imx.git - Freescale i.MX Linux Tree )
Can someone suggest a good WiFi module chipset also, which the i.MX6 supports with the kernel drivers.
I am a beginner on this so please bear with me if these are basics.

Outcomes