Fabien Jolimet

Upload file from web server to a 52235EVB board

Discussion created by Fabien Jolimet on Jun 19, 2008
Latest reply on Aug 13, 2008 by Nabeen Thakur
Hello,

I work on the board 52235EVB with codewarrior V7.0 and I am using the ColdFire TCP/IP Lite by InterNiche.

I would like to know if it is posible to upload a file from the web server to the board in order to load this file in an extern flash memory.
So I want to upload a file packet by packet in order to have the time to tranfert each packet to the extern memory flash.

I would like to do this in order to load a new application to the extern flash memory to load to the intern flash memory on the following reset.

Does anyone have an idea to do that ?

Thanks

Fabien

Outcomes