I use the mx6q development board, the kernel is linux3.0.35, SPI operation according to the information on the web, now in the SPI chip select signal line is sent every eight men
Pull high chip select signal, the next byte start signal until the end of eight low to high. I want to make a chip select signal to send data until the low level.
All data sent to the high end, how to configure??
Hi,
I do what you mean,I can field ECSPIx_CONREG[BURST_LENGTH] by SPI test program,but send byte over 32bit ,the kernel will crash.
Thanks for your early reply.
Best Regards, Lin Haibo
Hi
please set proper field ECSPIx_CONREG[BURST_LENGTH]
described in sect.21.7.3 Control Register (ECSPIx_CONREG)
i.MX6DQ Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------