P1021: GPIO: why CE_PB29 can not be controlled?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1021: GPIO: why CE_PB29 can not be controlled?

359 Views
carlpeng
Contributor II

Hello,

In my design, will use PB29 as an input pin to detect the status of the external device, but I find that even though I pull up the PB29 to almost 3.3v by a pull-up resistor, I still read the pin value as 0x0(read the value through GUTS_CPDAT register), why?

Could you please help to give some comments? Thanks a lot!

Meanwhile, I find some description as below in the P1021RM.pdf:

pastedImage_1.png

so,  PB29 can be controlled by the using GUTS_CPDIR2n, GUTS_CPDAT registers, not 

need to configure GUTS_PMUXCR, since from the above description, CE_PB[29 : 30] always functions as QE pins.

Thank you,

Carl

Labels (1)
0 Kudos
1 Reply

269 Views
alexander_yakov
NXP Employee
NXP Employee

Yes, your understanding is correct, QE pin PB29 is not shared with any other function, so you do not need to configure it in PMUXCR.

Please check GUTS_CPDIR and GUTS_CPPARB should be set to "10" and "00" respectively.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos