用LPC1768设计的板子,固件烧好以后,在windowsXP下,插入USB口,说需要驱动,驱动装好以后,就可以正常工作了。换了windows10,插入电脑后,也说需要驱动,但XP的驱动它不认。请问如果处理?
(Google translation into English follows:
With LPC1768 board design, firmware burned later in windowsXP, insert the USB port, said the need to drive, drive installed later, it can work properly.
Changed windows10, into the computer, also said that the need to drive, but the XP drivers do not recognize it.
Ask if the process?
)
请问解决了么?我们现在也遇到这个win10 64bit的驱动问题了
这个问题已困扰我们和客户几个月了,因以前使用致远公司zyUSBDrv(x86)的驱动,在32位系统下用 usb通过isp烧程序 现在新电脑win10只能使用笔记本win7电脑来编程和烧录,网上无有HID驱动适合,非常麻烦。正准备卸载win10恢复win7了,请提供下载链接,谢谢!
请问解决了么?我们现在也遇到这个win10 64bit的驱动问题了
您好!
我们用VC++6.0编写的上位机程序,通过USB和LPC1768的USB端口 ( 29和30脚的D+D-) 通信,
在windowsXP下,将USB线插入电脑后,提示安装驱动程序,驱动程序安装好之后,上下位机之间的通信正常。
在windows10下,将USB线插入电脑,也提示安装驱动程序,但操作系统不认驱动程序。
Hi,
请问你使用USB 通信的方式或者称为class的是HID呢,还是CDC?
还有你的驱动程序也是自己写的?
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
请问解决了么? 需要一组可用的 win10 64bit的驱动 动态链接库和.lib库等组件来替代原来致远提供的 32bit 的 zyUSBDrv.sys , zyUSBDrv.inf ,zyUSBDev.dll, zyUSBDev.lib, zyUSBDev.h ; 并提供 对IN端点进行读操作 以及 对OUT端点进行写操作 的API接口
Hi,
请问楼主使用是哪种USB 应用的例程呢?
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------