Code Warrior support for Flexis - free license?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior support for Flexis - free license?

506 Views
paulschoenke
Contributor III

Hello Community:

 

I have a legacy design to support with the Freescale Flexis MCUs.  Is the Code Warrior IDE no longer free for this?

Previously, this was free with the Code Warrior development environment at the 64kB (V1) or 32kB (S08) code size limitation. 


Any feedback or input is welcomed and appreciated!

Thanks again!

Paul

Labels (1)
0 Kudos
1 Reply

413 Views
TomasPaez
NXP Employee
NXP Employee

Here are the free editions from NXP 

Special Edition Software|NXP 

for S08 version used is 6.3, however there are some codesize limit on this free edition.

0 Kudos