Lollipop5.0.0 images not booting on iMXDL custome board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lollipop5.0.0 images not booting on iMXDL custome board

419 Views
vivektol
Contributor I

Hi,

          We have developed custom board with imx6dl processor by taking reference as SABRESD imx6q board.

-- Our emmc (16GB) is also connected to same SD4 port.

-- DRAM (4GB) is connected to DRMA pins.

-- External SDCard is conneted to SD3 port.

-- WiFi /BT (WL1831) is connected to SD1 and SD2 port.

We have developed images for this board as per

imx6 Android kitkat4.4.2 user guide and

imx6 Android Lollipop5.0.0 user guide.

We are using mfg tool available on NXP site for kitkat and Lollipop for downloading images onto the custom board.

On our custom board kitkat images are properly booting. But Lollipop images not booted. Even uboot also not started.

What may be the problem? Please guide.

Labels (3)
0 Kudos
1 Reply

349 Views
igorpadykov
NXP Employee
NXP Employee

Hi VIVEK

please run ddr test

https://community.freescale.com/docs/DOC-105652 

and rebuild uboot using new calibrations settings in *.cfg file.

http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2015.04_4.1.15_1.0.0_ga

for programming image use Lollipop mfg tools version found on

i.MX 6 Series Software and Development Tool|NXP 

Use Lollipop Docs

http://www.nxp.com/webapp/Download?colCode=IMX6_L5.1_2.1.0_ANDROID-DOCS&Parent_nodeId=13376994810717... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos