Hi,
I want to work with the factory trimming values but, as far as i understand, those values are not loaded into the ICS trim registers if BDM is active.
This means that during development, while i am working with a debugger, i can not get the device to run with the factory trim values.
Is there a way to read and load the factory trim values into the ICS trim registers?
I am working with CW10.6, MC9S08PA8, P&E Multilink debugger
Thanks,
Timor
CodeWarrior load the TRIM value by default when debug, and it's optional, you can turn off.
User should load by himself, example projects do this, too.
Hi
please also check this application note for more information about the ICS and the clock option on the S08
Clock Options on the HC9S08 Family
Regards
Vicente Gomez