Dear All,
We are using usdpaa uIamge and dtb file.
Ifconfig log
root@t2080rdb:/boot# ifconfig -a
fm1-mac9 Link encap:Ethernet HWaddr 00:04:9f:03:cb:62
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:8 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Memory:fe4f0000-fe4f0fff
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
macless0 Link encap:Ethernet HWaddr 00:11:22:33:44:55
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
sit0 Link encap:UNSPEC HWaddr 00-00-00-00-89-40-00-00-00-00-00-00-00-00-00-00
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
tunl0 Link encap:IPIP Tunnel HWaddr
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
We compiled fsl_sdk-v2.0 from the link: sdk/usdpaa/usdpaa-apps.git - User-Space Data-Path Acceleration Architecture Demo Applications
Compiled for the T2080RDB-PC and got ipfwd_app.
Trying to run binary and getting following log:
./ipfwd_app 1..7
Found /fsl,dpaa/ethernet@0, Tx Channel = 802, FMAN = 0, Port ID = 1
Found /fsl,dpaa/ethernet@1, Tx Channel = 803, FMAN = 0, Port ID = 2
Found /fsl,dpaa/ethernet@2, Tx Channel = 804, FMAN = 0, Port ID = 3
Found /fsl,dpaa/ethernet@3, Tx Channel = 805, FMAN = 0, Port ID = 4
Found /fsl,dpaa/ethernet@9, Tx Channel = 801, FMAN = 0, Port ID = a
Found /fsl,dpaa/ethernet@8, Tx Channel = 800, FMAN = 0, Port ID = 9
Found /fsl,dpaa/ethernet@10, MAC-LESS node
Configuring for 1 network interface
Allocated DMA region size 0x1000000
ipfwd_app starting
Message queue to send: /mq_snd_1612
Message queue to receive: /mq_rcv_1612
Configured 10G port @ FMAN:0, MAC:9 as IF_IDX:89
Released 0 bufs to BPID 17
Data stashing: Enabled
Thread uid:0 alive (on cpu 1)
Thread uid:1 alive (on cpu 2)
Thread uid:2 alive (on cpu 3)
Thread uid:3 alive (on cpu 4)
Thread uid:4 alive (on cpu 5)
Thread uid:5 alive (on cpu 6)
Thread uid:6 alive (on cpu 7)
cpu hotplug daemon not running: No such file or directory
We are not getting any Rx and Tx counter increment value.
Please let me know what is the process to step forward to see ipforwarding application.
Thanks,
Vidya